Scroll axes enabled
Which scroll axes to show if element is bigger than the control
- BrowseName
- ScrollAxesEnabledEnum
Values
| Value | DisplayName | Description |
|---|---|---|
| 0 | Both | Both axes are shown |
| 1 | X Axis | Only X Axis is shown |
| 2 | Y Axis | Only Y Axis is shown |
Which scroll axes to show if element is bigger than the control
| Value | DisplayName | Description |
|---|---|---|
| 0 | Both | Both axes are shown |
| 1 | X Axis | Only X Axis is shown |
| 2 | Y Axis | Only Y Axis is shown |
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.