Reference time zone
Time zone for displaying the date and time on the X axis. (UTC: time zone standard; Locale: time zone of the device from which the data is generated; Session: session time zone). To record the data displayed in local time zone, enable the Log Local Time property of the Data logger object
- BrowseName
- ReferenceTimeZone
Values
| Value | DisplayName | Description |
|---|---|---|
| 0 | UTC | Time zone standard |
| 1 | Local | Time zone of the device from which the data is generated |
| 2 | Session | Session time zone |