Position
Alignment of the control to the container
- BrowseName
- Position
Values
| Value | DisplayName | Description |
|---|---|---|
| 0 | Top left | Element is docked to the top left corner |
| 1 | Top center | Element is docked to the center of the top border |
| 2 | Top right | Element is docked to the top right corner |
| 3 | Left center | Element is docked to the center of the left border |
| 4 | Center | Element is centered (vertically and horizontally) to the container |
| 5 | Right center | Element is docked to the center of the right border |
| 6 | Bottom left | Element is docked to the bottom left corner |
| 7 | Bottom center | Element is docked to the center of the bottom border |
| 8 | Bottom right | Element is docked to the bottom right corner |