Position
Position of the scale relative to the control
- BrowseName
- PositionEnum
Values
| Value | DisplayName | Description |
|---|---|---|
| 0 | Left | Scale is on the left of the control (only if orientation is set to Vertical) |
| 1 | High | Scale is above the control (only if orientation is set to Horizontal) |
| 2 | Right | Scale is on the right of the control (only if orientation is set to Vertical) |
| 3 | Low | Scale is below the control (only if orientation is set to Horizontal) |