Digital alarm
Monitors Boolean variables. Activates when the value of the monitored variable is not the normal state value
- BrowseName
- OffNormalAlarmController
- SuperType
- AlarmController(AlarmController)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Normal state value | NormalStateValue | Double | Normal value for the monitored variable. The alarm activates when the value of the variable monitored is different from this |
| Enabled | Enabled | Boolean | (Inherited from AlarmController) |
| Active | Active | Boolean | (Inherited from AlarmController) |
| Auto acknowledge | AutoAcknowledge | Boolean | (Inherited from AlarmController) |
| Auto confirm | AutoConfirm | Boolean | (Inherited from AlarmController) |
| Input variable | InputValue | Double | (Inherited from AlarmController) |
| Message | Message | LocalizedText | (Inherited from AlarmController) |
| Severity | Severity | UInt16 | (Inherited from AlarmController) |
| Max TimedShelve duration | MaxTimeShelved | Duration | (Inherited from AlarmController) |
| Preset TimedShelve duration | PresetTimeShelved | Duration | (Inherited from AlarmController) |
| Last event | LastEvent | BaseDataType | (Inherited from AlarmController) |
| Shelved | Shelved | Boolean | (Inherited from AlarmController) |
Events
OffNormalAlarmType
- BrowseName
- OffNormalAlarmType