Exclusive limit alarm

BrowseName
ExclusiveLimitAlarmController
SuperType
Limit alarm(LimitAlarmController)

Properties

Name BrowseName DataType Description
High-high limit HighHighLimit Double (Inherited from Limit alarm)
High limit HighLimit Double (Inherited from Limit alarm)
Low limit LowLimit Double (Inherited from Limit alarm)
Low-low limit LowLowLimit Double (Inherited from Limit alarm)
Active Active Boolean (Inherited from Limit alarm)
Message Message LocalizedText (Inherited from Limit alarm)
Enabled Enabled Boolean (Inherited from AlarmController)
Auto acknowledge AutoAcknowledge Boolean (Inherited from AlarmController)
Auto confirm AutoConfirm Boolean (Inherited from AlarmController)
Input variable InputValue Double (Inherited from AlarmController)
Severity Severity UInt16 (Inherited from AlarmController)
Max TimedShelve duration MaxTimeShelved Duration (Inherited from AlarmController)
Preset TimedShelve duration PresetTimeShelved Duration (Inherited from AlarmController)
Last event LastEvent BaseDataType (Inherited from AlarmController)
Shelved Shelved Boolean (Inherited from AlarmController)