Exclusive deviation alarm
Monitors the deviation from a setpoint value of variables relating to physical quantities. Activates when the value of the monitored variable has a deviation equal to or greater than the set value. When several deviation limits are reached consecutively, the alarm signals only the last limit reached
- BrowseName
- ExclusiveDeviationAlarmController
- SuperType
- Exclusive limit alarm(ExclusiveLimitAlarmController)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Set point value | Setpoint | Double | Ideal value for the monitored variable |
| High-high limit | HighHighLimit | Double | (Inherited from Limit alarm) |
| High limit | HighLimit | Double | (Inherited from Limit alarm) |
| Low limit | LowLimit | Double | (Inherited from Limit alarm) |
| Low-low limit | LowLowLimit | Double | (Inherited from Limit alarm) |
| Active | Active | Boolean | (Inherited from Limit alarm) |
| Message | Message | LocalizedText | (Inherited from Limit alarm) |
| Enabled | Enabled | Boolean | (Inherited from AlarmController) |
| Auto acknowledge | AutoAcknowledge | Boolean | (Inherited from AlarmController) |
| Auto confirm | AutoConfirm | Boolean | (Inherited from AlarmController) |
| Input variable | InputValue | Double | (Inherited from AlarmController) |
| Severity | Severity | UInt16 | (Inherited from AlarmController) |
| Max TimedShelve duration | MaxTimeShelved | Duration | (Inherited from AlarmController) |
| Preset TimedShelve duration | PresetTimeShelved | Duration | (Inherited from AlarmController) |
| Last event | LastEvent | BaseDataType | (Inherited from AlarmController) |
| Shelved | Shelved | Boolean | (Inherited from AlarmController) |
Events
ExclusiveDeviationAlarmType
- BrowseName
- ExclusiveDeviationAlarmType