Exclusive level alarm
Monitors when the values of interest are reached for variables relating to physical quantities. Activates when the value of the monitored variable reaches one or more limits of interest. When several limits of interest are reached consecutively, the alarm signals only the last limit reached
- BrowseName
- ExclusiveLevelAlarmController
- SuperType
- Exclusive limit alarm(ExclusiveLimitAlarmController)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| High-high limit | HighHighLimit | Double | (Inherited from Limit alarm) |
| High limit | HighLimit | Double | (Inherited from Limit alarm) |
| Low limit | LowLimit | Double | (Inherited from Limit alarm) |
| Low-low limit | LowLowLimit | Double | (Inherited from Limit alarm) |
| Active | Active | Boolean | (Inherited from Limit alarm) |
| Message | Message | LocalizedText | (Inherited from Limit alarm) |
| Enabled | Enabled | Boolean | (Inherited from AlarmController) |
| Auto acknowledge | AutoAcknowledge | Boolean | (Inherited from AlarmController) |
| Auto confirm | AutoConfirm | Boolean | (Inherited from AlarmController) |
| Input variable | InputValue | Double | (Inherited from AlarmController) |
| Severity | Severity | UInt16 | (Inherited from AlarmController) |
| Max TimedShelve duration | MaxTimeShelved | Duration | (Inherited from AlarmController) |
| Preset TimedShelve duration | PresetTimeShelved | Duration | (Inherited from AlarmController) |
| Last event | LastEvent | BaseDataType | (Inherited from AlarmController) |
| Shelved | Shelved | Boolean | (Inherited from AlarmController) |
Events
ExclusiveLevelAlarmType
- BrowseName
- ExclusiveLevelAlarmType