Variables
A variable is an attribute of an object. Assign a value to a variable to display the value at runtime.
View variables from either:
- Project view. Navigate to the folder containing the variables. The UI folder cannot contain variables.
- Properties. Select an object, type, or variable in Project view or select and object in the editor. The variables or properties for the selected item appear in Properties.
- Array editor
- Create a variable
- Create an analog variable
- Create a node pointer
- Create a variable type
- Create a variable from a type
- Set the unit of measure for a variable
- Change the unit of measure for a variable
- Remove the unit of measure from a variable
- Add a range to a variable
- Delete a range from a variable