Change the unit of measure for a variable
Change the unit of measure for a variable that displays at runtime.
- In Project view, select a variable.
- In Properties, select the unit of measurement in the value of the variable.
- Select the unit of measure for the variable value and choose Select.
The unit of measure appears in the value for the variable.