Create a variable
Create a variable in Project view.
- In Project view, select the folder or object to contain the variable.
-
In the Project view toolbar, select
Add new and then select Variable.
-
(optional) To change the variable data type, in Properties, next to the variable name, select the existing data type and then select another data type.
Tip:
If you do not see the required option, select Show all. Start typing to select the item to find.
To define an array, select Array and then enter the array dimensions. Enter 0 to create an unconstrained array.
-
In Properties, select
and enter a value for the variable or create a dynamic link.
If you edit an array variable value, the Array editor displays. For more information, see Array editor.
For more information about dynamic links, see Create dynamic links.
-
(optional) In Properties, select
, select Display name, and enter the display name.
-
(optional) In Properties, select
, select Description, and enter the description.
- (optional) Set the unit of measure for a variable.
- (optional) Add a range to a variable.