Paths
You can use path shortcuts when developing your application logic.
| Shortcut | Description |
|---|---|
|
%PROJECTDIR% |
A directory that contains files transferred at runtime (images, documents, and so on). Example: C:\Users\UserName\Documents\Rockwell Automation\FactoryTalk Optix\ProjectName |
|
%APPLICATIONDIR% |
A directory that contains objects used at runtime, including these objects:
|
|
%USBN%, where N is a number associated with the USB device. |
A path to a specific USB device connected to the target device. |