Objects
An object is an element that represents a physical or non-physical component in the project. A type is a model or template object for creating instances of an object.
Create objects from Project view or Type view. Change the properties of an object to change the appearance and data values displayed for that object at runtime.
To create objects: