Create a variable from a type
Create a variable from a type to have the type automatically assigned to the variable that you create.
- In Type view, navigate to the folder that contains the variable type.
-
From Type view, drag the variable type into Project view.
An instance of the variable type displays in Project view.
-
(optional) In Properties, select
, select Display name, and enter the display name.
-
(optional) In Properties, select
, select Description, and enter the description.