Create a variable type
Create a variable type in Project view. You can then create variables of the variable type.
-
From Project view, drag an existing variable into a folder in Type view.
The variable type appears in both Type view and in the Project view folder that has the same name as the folder in Type view.Tip: The variable in Project view is appended with (type) and the original variable that you dragged from Project view is now an instance of the type.
-
(optional) In Properties, select
, select Display name, and enter the display name.
-
(optional) In Properties, select
, select Description, and enter the description.