Remove the unit of measure from a variable
Remove the unit of measure for a variable to no longer have the value for that variable appear in that unit of measure.
- In Project view, select a variable.
- In Properties, select the unit of measurement in the value of the variable.
- Select <None> and then choose Select.
The unit of measure is removed from the variable.