Create a node pointer
Create a node pointer in Project view to reference to another node of the project.
- In Project view, select the folder or object to contain the variable.
-
In Properties, create a dynamic link to the node to point to.
For more information about dynamic links, see Create dynamic links.
-
(optional) expand NodePointer# and complete these properties:
- Kind. The kind of the node that the node pointer targets.
- Node class. Either:
- Instance
- Type
- Any
-
(optional) In Properties, select
, select Display name, and enter the display name.
-
(optional) In Properties, select
, select Description, and enter the description.