View alarms in UTC time zone
Alias the Time property of the Alarm grid object to view events in the UTC (Coordinated Universal Time) time zone standard. UTC is the time standard on which all time zones are based worldwide. Viewing alarms in the UTC time zone ensures that all users are seeing the same time stamps for the alarms.
-
In the main toolbar, select
Template Libraries.
- In Template Libraries, select Widgets.
-
Drag the Alarms Grid object to the desired folder in the UI folder.
AlarmGrid# (type) appears.
- In Template Libraries, select Close.
-
In the editor, select the alarm grid and then in Properties:
- Expand Timestamp.
- Expand the Data grid category.
- Expand the Column category and then select DataItemTemplate.
-
In Text, select
Add Dynamic Link.
- In the Dynamic Links window, expand Aliases.
- Expand Alarm Condition and then select Time.
- Choose Select.