Create an alarm type
Create and configure a custom alarm type to be able to create instances of the alarm type instead of creating multiple alarms that have different values for the same graphic object. Create custom properties for an alarm type to monitor different values from the different instances of the alarm in the Alarm grid.
Prerequisites
To create an alarm type
-
(optional) Add a custom property:
- In Type view, expand Alarms.
- Drag the alarm object from Project view into Alarms in Type view.
The new alarm type has the suffix (type)
and appears in Project view in the same folder as the original alarm. The original alarm is now an instance of the new type.