Create a dynamic alarm message
Create an alarm message that appears at runtime when the alarm is active. For example, create a message that indicates a flow rate or level is dangerously low when the alarm is active.
Prerequisites
To create a dynamic alarm message
- In Project view, select the alarm.
-
In Properties, in Message, select
Add Dynamic Link, and then select Advanced.
-
In the Dynamic Link Editor, in Message, select
and then select String formatter.
-
In Dynamic Link, select
Change Dynamic Link.
- Specify the Input value of the alarm as the source for the Dynamic Link.
- In Format, enter the text of the alarm message, using the placeholder {0} to identify the value of the source variable.
-
Select
as necessary to set the direction of the link.