Alarm filters
By default, the Alarm grid widget displays all enabled and active alarms. Queries filter alarms at runtime to display only certain alarms.
Additional alarm queries could:
- Display only the row of the Motor5 object. The query would be SELECT * FROM Model WHERE BrowseName = 'Motor5'
- Display only the rows of objects with an Acceleration of 20. The query would be SELECT * FROM Model WHERE Acceleration = 20
- Display the rows of objects with Acceleration greater than 20 and Speed from 30 to 500. The query would be SELECT * FROM Model WHERE Acceleration > 20 AND Speed BETWEEN 30 AND 500
- Display objects with BrowseName that start with Faulty. The query would be SELECT * FROM Model WHERE BrowseName LIKE 'Faulty%'