Create an alarm
Create an alarm to specify which value generates an alarm at runtime.
-
In Project view, right-click Alarms, select New, and then select the alarm type.
The alarm appears in Alarms.
- With the alarm selected, in Properties, in Input variable, enter or link to the variable to monitor.
-
Depending on the alarm type, set the normal value status or limits.
A property value displays Not set when the normal value or limit is not entered.
-
In Message, enter the message to display when the alarm event occurs.
For Exclusive and Non-Exclusive alarm types, you can additionally set a separate message for each alarm state.
- In Severity, enter the alarm priority level from 1 to 1000.
- In Enabled, select True. Enabled is the default.