Create an Analog alarm grid
Create an Analog alarm grid to display the status of each alarm in a row, including the High, HighHigh, Low, or LowLow values.
Customize the objects included in the Analog alarm grid to change the appearance of the grid and display specific alarm information.
-
In the main toolbar, select
Template Libraries.
- In Template Libraries, select Widgets.
-
Under Components, drag Analog Alarm Grid to a folder in the UI folder.
AnalogAlarmGrid# (type) appears.
- In Template Libraries, select Close.
-
(optional) On the editor, select the alarm grid and the buttons of the alarm grid to customize the Properties and Events of the grid and buttons. For example, to change the appearance of the grid:
- Row color. Select the background color row or select
Add Dynamic Link to bind to a tag with the value of the color. - Row text color, Select the color of the text in the alarm grid or select
Add Dynamic Link to bind to a tag with the value of the color.
- Row color. Select the background color row or select
-
(optional) To display additional alarm information at runtime, select AlarmsDataGrid and add columns: