Set dynamic variables polling time for alarms
Set the time interval between readings of variable values from OPC UA servers and tag values from controllers.
- In Project view, select the root project node.
-
In Properties, set Dynamic variables polling time.
Tip: Set the polling time between one sampling and the next in HHHH:MM:SS.MS format.