Panel section
Fixed-size section of a Report object
- BrowseName
- PanelSection
- SuperType
- Panel(Panel)
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
HorizontalAlignment | Horizontal alignment | ||
VerticalAlignment | Vertical alignment | ||
Width | Size | ||
Height | Size | ||
LeftMargin | Size | ||
RightMargin | Size | ||
TopMargin | Size | ||
BottomMargin | Size | ||
Enabled | Boolean | ||
HitTestVisible | Boolean | ||
Rotation | Size | ||
Opacity | Float | ||
MoveTarget | NodeId | ||
Visible | Visible | Boolean | (Inherited from Element) |