PDF generated

The Generate PDF method of a Report object was run

BrowseName
GeneratePdfCompletedEvent
SuperType
BaseEventType(BaseEventType)

Properties

Name BrowseName DataType Description
Output file OutputPath ResourceUri Location in the file system where the PDF file is to be saved (for example, %APPLICATIONDIR%/MyReport.pdf)
Result Result PDF generation result Result of the PDF print. 0: PDF generated successfully; 1: locale not supported; 2: failed to process template; 3: unable to overwrite output file; 4: unable to generate PDF; 5: Resource output URI empty or invalid
Operation ID OperationId Guid Locale of the report contents
EventId ByteString (Inherited from BaseEventType)
EventType NodeId (Inherited from BaseEventType)
SourceNode NodeId (Inherited from BaseEventType)
SourceName String (Inherited from BaseEventType)
Time UtcTime (Inherited from BaseEventType)
ReceiveTime UtcTime (Inherited from BaseEventType)
LocalTime TimeZoneDataType (Inherited from BaseEventType)
Message LocalizedText (Inherited from BaseEventType)
Severity UInt16 (Inherited from BaseEventType)
ConditionClassId NodeId (Inherited from BaseEventType)
ConditionClassName LocalizedText (Inherited from BaseEventType)
ConditionSubClassId NodeId (Inherited from BaseEventType)
ConditionSubClassName LocalizedText (Inherited from BaseEventType)