SessionDiagnosticsVariableType
- BrowseName
- SessionDiagnosticsVariableType
- SuperType
- Variable(BaseDataVariableType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| SessionId | NodeId | ||
| SessionName | String | ||
| ClientDescription | ApplicationDescription | ||
| ServerUri | String | ||
| EndpointUrl | String | ||
| LocaleIds | LocaleId | ||
| ActualSessionTimeout | Duration | ||
| MaxResponseMessageSize | UInt32 | ||
| ClientConnectionTime | UtcTime | ||
| ClientLastContactTime | UtcTime | ||
| CurrentSubscriptionsCount | UInt32 | ||
| CurrentMonitoredItemsCount | UInt32 | ||
| CurrentPublishRequestsInQueue | UInt32 | ||
| TotalRequestCount | ServiceCounterDataType | ||
| UnauthorizedRequestCount | UInt32 | ||
| ReadCount | ServiceCounterDataType | ||
| HistoryReadCount | ServiceCounterDataType | ||
| WriteCount | ServiceCounterDataType | ||
| HistoryUpdateCount | ServiceCounterDataType | ||
| CallCount | ServiceCounterDataType | ||
| CreateMonitoredItemsCount | ServiceCounterDataType | ||
| ModifyMonitoredItemsCount | ServiceCounterDataType | ||
| SetMonitoringModeCount | ServiceCounterDataType | ||
| SetTriggeringCount | ServiceCounterDataType | ||
| DeleteMonitoredItemsCount | ServiceCounterDataType | ||
| CreateSubscriptionCount | ServiceCounterDataType | ||
| ModifySubscriptionCount | ServiceCounterDataType | ||
| SetPublishingModeCount | ServiceCounterDataType | ||
| PublishCount | ServiceCounterDataType | ||
| RepublishCount | ServiceCounterDataType | ||
| TransferSubscriptionsCount | ServiceCounterDataType | ||
| DeleteSubscriptionsCount | ServiceCounterDataType | ||
| AddNodesCount | ServiceCounterDataType | ||
| AddReferencesCount | ServiceCounterDataType | ||
| DeleteNodesCount | ServiceCounterDataType | ||
| DeleteReferencesCount | ServiceCounterDataType | ||
| BrowseCount | ServiceCounterDataType | ||
| BrowseNextCount | ServiceCounterDataType | ||
| TranslateBrowsePathsToNodeIdsCount | ServiceCounterDataType | ||
| QueryFirstCount | ServiceCounterDataType | ||
| QueryNextCount | ServiceCounterDataType | ||
| RegisterNodesCount | ServiceCounterDataType | ||
| UnregisterNodesCount | ServiceCounterDataType |