ServerDiagnosticsSummaryType
- BrowseName
- ServerDiagnosticsSummaryType
- SuperType
- Variable(BaseDataVariableType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| ServerViewCount | UInt32 | ||
| CurrentSessionCount | UInt32 | ||
| CumulatedSessionCount | UInt32 | ||
| SecurityRejectedSessionCount | UInt32 | ||
| RejectedSessionCount | UInt32 | ||
| SessionTimeoutCount | UInt32 | ||
| SessionAbortCount | UInt32 | ||
| PublishingIntervalCount | UInt32 | ||
| CurrentSubscriptionCount | UInt32 | ||
| CumulatedSubscriptionCount | UInt32 | ||
| SecurityRejectedRequestsCount | UInt32 | ||
| RejectedRequestsCount | UInt32 |