System
Enables read/write at runtime for some system settings of the network interfaces
- BrowseName
- System
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Reboot required | RebootRequired | Boolean | Requires a device reboot to commit system configuration changes |
| Network interfaces | NetworkInterfaces | Network interface | List of the network interfaces |
| Date and time | DateAndTime | Date and time configuration | |
| Device | Device | Device status and configuration | |
| Display | Display | Device display status and configuration | |
| Application | Application | Application status and configuration |
Methods
Reboot
- BrowseName
- Reboot
Restart the system. For supported operating systems, verify if the user running the FactoryTalk Optix Application has the authorization to perform the operating system restart
Load application
- BrowseName
- LoadApplication
Load application onto device
| Name | DataType | Description |
|---|---|---|
| FilePath | AbsoluteResourceUri | FilePath |
| Password | String | Password |
| DeleteApplicationFiles | Boolean | DeleteApplicationFiles |
| Name | DataType | Description |
|---|---|---|
| Result | Boolean | LoadApplicationResult |