Network interface
Configure the WAN and LAN network interfaces
- BrowseName
- NetworkInterface
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| DHCP activated | DHCPClientEnabled | Boolean | Obtain IP settings automatically using DHCP |
| IP address | IPAddress | String | IP address of the network |
| DNS 1 | DNS1 | String | Primary DNS address of the network |
| DNS 2 | DNS2 | String | Secondary DNS address of the network |
| Default gateway | DefaultGateway | String | IP address of the default network gateway |