FTRemoteAccess
FactoryTalk Remote Access connection
- BrowseName
- FTRemoteAccess
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Runtime version | RuntimeVersion | String | Version of FactoryTalk Remote Access runtime |
| Server connection | ServerConnection | ServerConnectionEnum | Status of the device connection to FactoryTalk Remote Access server (0=Disconnected, 1=Connecting, 2=Connected) |
| Registered to domain | RegisteredToDomain | Boolean | Indicates that the device is registered to the FactoryTalk Remote Access domain |
| Assistance request mode | AssistanceRequestMode | AssistanceRequestModeEnum | Submit assistance requests mode (0=Disabled, 1=Enabled, 2=ContactDetailsRequired) |
| Assistance requested | AssistanceRequested | Boolean | Indicates that assistance has been requested |
| Remote connection count | RemoteConnectionCount | UInt32 | Number of remote connections to the device |
| Anonymous id | AnonymousId | String | ID credential needed to add device to FTRA domain |
| Anonymous password | AnonymousPassword | String | Password credential required to add device to FactoryTalk Remote Access domain |
Methods
Connect to server
- BrowseName
- ConnectToServer
Connects the device to the FactoryTalk Remote Access server
| Name | DataType | Description |
|---|---|---|
| Result | Boolean | Result code of the connection to the FactoryTalk Remote Access server(s) |
Disconnect from server
- BrowseName
- DisconnectFromServer
Disconnects the device from the FactoryTalk Remote Access server
| Name | DataType | Description |
|---|---|---|
| Result | Boolean |
Open assistance request
- BrowseName
- OpenAssistanceRequest
Opens a request for remote assistance
| Name | DataType | Description |
|---|---|---|
| Name | String | User name of who opened the remote assistance request |
| ContactInformation | String | Contact information of who opened the remote assistance request |
| Description | String | Brief description of the assistance request |
| Name | DataType | Description |
|---|---|---|
| Result | OpenAssistanceRequestResultEnum | Result of the remote assistance request |
Close assistance request
- BrowseName
- CloseAssistanceRequest
Closes a request for remote assistance
| Name | DataType | Description |
|---|---|---|
| Result | CloseAssistanceRequestResultEnum | Closes an assistance request that has been previously opened from the current device |
Approve incoming remote connection
- BrowseName
- ApproveIncomingRemoteConnection
Approves an incoming FactoryTalk Remote Access connection
| Name | DataType | Description |
|---|---|---|
| SupervisorId | ByteString | ID of the supervisor of the remote connection request |
| Name | DataType | Description |
|---|---|---|
| Result | IncomingRemoteConnectionApprovalResultEnum | Result code of the remote connection approval |
Deny incoming remote connection
- BrowseName
- DenyIncomingRemoteConnection
Denies an incoming FactoryTalk Remote Access connection
| Name | DataType | Description |
|---|---|---|
| SupervisorId | ByteString | ID of the supervistor of the remote connection after it is denied |
| Name | DataType | Description |
|---|---|---|
| Result | IncomingRemoteConnectionApprovalResultEnum | Result code of the remote connection approval |
Events
Remote Connection Request
- BrowseName
- Remote Connection Request
Executes a method when an incoming FactoryTalk Remote Access connection occurs