Configure a spin box
Add a spin box object and edit its properties.
- In Project view, in UI, right-click a container to contain the spin box, and then select .
-
(optional) In Properties, adjust the spin box settings:
-
Value. Starting value. Either a numerical value or a dynamic link to a variable with a numerical value.
For more information about dynamic links, see Create dynamic links.
-
Minimum value. Minimum value that you can set for the spin box.
Tip: If the value is outside the Minimum value and Maximum value range, the spin box border turns red for a brief moment and the value reverts to the previous value. -
Maximum value. Maximum value that you can set for the spin box.
-
Increment. Value by which to increase or decrease the value when you use the buttons to increment the value.
-
Input format. Format of displayed value.
-
Editable. Enable entering the spin box value with keyboard keys.
Tip: Even if Editable is set to False, you can still use spin box buttons to increase or decrease the spin box value. -
Show buttons. Display buttons to increase or decrease the value.
-