Momentary button
Generates events to perform methods. Includes Minimum hold time and Maximum hold time properties.
Events
Use these button events to trigger methods:
| Event | Generated at runtime when |
|---|---|
|
MouseClick event |
An object is clicked or touched and then released. |
|
MouseDown event |
An object is clicked or touched. Use these methods to configure the behavior of the MouseDown event:
|
|
MouseUp event |
The click or touch of the object is released. |
Example