Base controls
Use base controls objects to implement user interface elements that enable interaction with the application.
| Object | Description |
|---|---|
| Label | Displays text that describes an item. |
| Text box | Inserts and displays text at runtime. |
| Spin box | Increases or decreases a numerical value using buttons or keys. |
| Editable label | Displays an editable description of an item. |
| LED | Displays a Boolean value in the form of an on LED or an off LED. |
| Button | Generates events to perform methods. |
| Switch | Sets and displays a Boolean value. |
| Checkbox | Sets and displays a Boolean value using select and clear. |
| Option button | Selects a mutually exclusive option in a group. |
| Linear gauge | Sets or displays an integer value within a range of possible values. |
| Circular gauge | Sets or displays an integer value within a range of possible values. |
| Date and time | Displays date and time data in a specific input format. |
| Duration | Displays the duration data. |