Linear gauge
Sets or displays an integer value within a range of possible values.
Use case
Set or display the value of an analog variable within a minimum and maximum value.
Tip: Use the Tooltip property to show or hide the display of the value above the selection point on the gauge. Use the Warning zone property to display specific ranges of values in different colors.
Example