Toggle button
Generates events to perform methods. Includes a Modified value event.
Events
Use these button events to trigger methods:
| Event | Generated at runtime when |
|---|---|
|
Modified value |
|
|
MouseClick event |
An object is clicked or touched and then released. |
|
MouseDown event |
An object is clicked or touched. |
|
MouseUp event |
The click or touch of the object is released. |
Example