Delayed button
Generates events to perform methods. Includes a MouseLongPress event.
Events
Use these button events to trigger methods:
| Event | Generated at runtime when |
|---|---|
|
MouseLongPress event |
An object is clicked or touched for the time specified in the Delay property. |
|
MouseClick event |
An object is clicked or touched and then released. |
|
MouseDown event |
An object is clicked or touched. |
|
MouseUp event |
The click or touch of the object is released. |
Example