Protect graphic objects with a password
Protect a container or a drawing with a password to prevent other FactoryTalk Optix Studio users from editing the protected object children.
Important: Protecting graphic objects with a password may not prevent advanced users from bypassing the object protection and should not be considered a safety or intellectual property protection.
- In Project view, right-click a container or drawing object to protect.
- Select .
- Enter a password.
-
(optional) Select
Show password to verify that you entered the password correctly.
- Select OK.
In Project view and in the Editor,
appears next to the password protected object. The child objects are hidden in Project view and cannot be edited.