Lock graphic objects protected with a password
Lock a password-protected graphic object to prevent other FactoryTalk Optix Studio users from editing child objects of the protected object.
In Project view or in the Editor, next to the object to lock, select
.
In Project view and in the Editor,
appears next to the password protected object. The child objects are hidden in Project view and cannot be edited.