Create a graphic object from a type
Create an instance of an object from a predefined graphic object type or a custom graphic object type.
-
In Project view, in UI, double-click the container to contain the object.
The container opens in the editor.
-
From Type view, select the folders to navigate to the object type and then and drag the object to the editor.
Tip: You can also right-click a container in Project view and select the object to add from the New context menu.