Enable or disable a graphic object
Enable or disable an object. At runtime, users can interact with enabled objects.
- In Project view or in the editor, select the object to enable.
-
In Properties, in Enabled, select either:
- True. The object allows user interaction at runtime.
- False. The object prevents user interaction at runtime.