Animate a graphic object
Add and configure number, sequential, or parallel animation properties to animate an object.
- In Project view, select the object to animate.
-
In Properties, at the top, select
and then select either:
- Number animation. Animate objects by changing the value to another value over specific time.
- Sequential animation. Animate objects with a simple transition in the serial mode.
- Parallel animation. Animate object with a simple transition in the parallel mode.
Tip: You can also right-click a property that supports animations and select . - Configure animation properties. See Animation properties.