Configure an alarm log
An alarm log displays the date and time alarms occurred in your system as well as the state of each alarm.
-
In the main toolbar, select
Template Libraries and then select Misc.
-
Under Components, drag the Alarms Events Logger object into the Loggers folder of Project view.
AlarmsEventerLogger# appears.
- In Template Libraries, select Close.
- In Project view, drag the desired database object to the value of the logger Database property. The database is associated with the logger.
-
Select
Template Libraries and then select Widgets.
-
Drag Alarm Grid or Alarm History Grid with filter widget into the folder in Project view.
The new widget appears.
-
From Project view, drag the logger into Properties in AlarmsEventLogger.
Data that the log records at runtime will now be visible.
- (optional) To customize the graphical appearance of the widget, customize the data grid, date and time, button, and text color on the widget.