Automatically confirm and acknowledge alarms
Reduce the interaction required to manage alarms at runtime. Have the application confirm and acknowledge alarms automatically.
- In Project view, select the Alarm grid.
- In Properties, configure:
- Auto confirm. Select True to confirm that the issues causing alarms are resolved at runtime automatically. The Alarm grid displays only active and unacknowledged alarms.
- Auto acknowledge. Select True to acknowledge alarms at runtime automatically. The Alarm grid displays only unacknowledged alarms.
Tip: To have the Alarm grid display only active alarms at runtime, in Properties for the grid, set both Auto confirm and Auto acknowledge to True.