LoadApplicationStatusEventEnum
LoadApplicationStatusEventEnum
- BrowseName
- LoadApplicationStatusEventEnum
Values
| Value | DisplayName | Description |
|---|---|---|
| 0 | Success | Success |
| 1 | Internal error | Internal error |
| 2 | Invalid file path | Invalid file path |
| 3 | Invalid project descriptor file | Invalid project fescriptor file |
| 4 | Invalid project file | Invalid project file |
| 6 | Protection mode enabled | Protection mode enabled |
| 7 | Unencrypted file | Unencrypted file |
| 8 | Incorrect password | Incorrect password |
| 9 | Import already in progress | Import already in progress |