Recipe application event
An event which is triggered when the current recipe is applied
- BrowseName
- RecipeApplicationEvent
- SuperType
- AuditUpdateMethodEventType(AuditUpdateMethodEventType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Recipe name | RecipeName | String | Name of the recipe to be processed |
| Destination node | DestinationNode | NodeId | Destination of the recipe parameter |
| MethodId | NodeId | (Inherited from AuditUpdateMethodEventType) | |
| InputArguments | BaseDataType | (Inherited from AuditUpdateMethodEventType) | |
| ActionTimeStamp | UtcTime | (Inherited from AuditEventType) | |
| Status | Boolean | (Inherited from AuditEventType) | |
| ServerId | String | (Inherited from AuditEventType) | |
| ClientAuditEntryId | String | (Inherited from AuditEventType) | |
| ClientUserId | String | (Inherited from AuditEventType) | |
| EventId | ByteString | (Inherited from BaseEventType) | |
| EventType | NodeId | (Inherited from BaseEventType) | |
| SourceNode | NodeId | (Inherited from BaseEventType) | |
| SourceName | String | (Inherited from BaseEventType) | |
| Time | UtcTime | (Inherited from BaseEventType) | |
| ReceiveTime | UtcTime | (Inherited from BaseEventType) | |
| LocalTime | TimeZoneDataType | (Inherited from BaseEventType) | |
| Message | LocalizedText | (Inherited from BaseEventType) | |
| Severity | UInt16 | (Inherited from BaseEventType) | |
| ConditionClassId | NodeId | (Inherited from BaseEventType) | |
| ConditionClassName | LocalizedText | (Inherited from BaseEventType) | |
| ConditionSubClassId | NodeId | (Inherited from BaseEventType) | |
| ConditionSubClassName | LocalizedText | (Inherited from BaseEventType) |