OMRON Fins Station
Object that represents an OMRON Fins PLC
- BrowseName
- OmronFinsStation
- SuperType
- Communication station(CommunicationStation)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Maximum job size in bytes | MaximumJobSizeInBytes | UInt32 | Maximum size of a transmission of tags from the controller (in bytes). 0 = 1024 bytes (maximum value) |
| Maximum gap in bytes | MaximumGapInBytes | UInt32 | Maximum distance in bytes between two tags to be part of the same transmission |
| Source Network Address | SourceNetworkAddress | Byte | Default value = 0. It corresponds to the FINS parameter named Network Address. It can be set to 0 if the PC and all the devices are on the same network. The range of valid values is: 0..127 |
| Source Node Address | SourceNodeAddress | Byte | Default value = 50. It corresponds to the FINS parameter named Node Address. The range of valid values is: 0..254. Usually it corresponds to the last octet of the PLC Ethernet card IP address, i.e. if 192.168.0.54 is the PLC IP address, use 54 as node number |
| Source Unit Address | SourceUnitAddress | Byte | Default value = 0. It corresponds to the FINS parameter named Unit Address. If the communication is with the PLC CPU, the Unit Number should be 0 |
| IP address | IPAddress | String | Unique address to reach the controller on the network |
| Port | Port | UInt16 | Default value = 9600. This is the number of the TCP port of the device to be connected to. Valid port numbers range from 1 to 65535. Since FINS protocol requires that the source and destination port number be the same, if this parameter is modified, the Local Bound Port parameter should be modified as well and the two values must be equal |
| Timeout | Timeout | Duration | Maximum wait time in milliseconds to receive a response from the controller |
| Optimization type | OptimizationType | Optimization type | Select Datablock when working with consecutive addresses. Mixed Data otherwise |
| Operation code | OperationCode | Communication operation code | (Inherited from Communication station) |
| Tags | Tags | Folder | (Inherited from Communication station) |
| Types | Types | (Inherited from Communication station) |