OMRON Fins Tag
- BrowseName
- OmronFinsTag
- SuperType
- Tag(Tag)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Memory area | MemoryArea | Memory area | Controller memory location in which to read/write the tags |
| Data conversion | DataConversion | Data conversion | |
| BCD format | BCDFormat | BCD format | |
| Maximum length | MaximumLength | Int32 | (string data only) Maximum number of characters in the string |
| Word address | NumWord | UInt32 | Address in the memory location in which to read/write the tags |
| Bit number | BitOffset | UInt32 | Specify the position of the bit in the word |
| Flag address | NumFlag | UInt32 | |
| Bank number | BankNumber | UInt32 | |
| Array update mode | ArrayUpdateMode | Tag array update mode | (Inherited from Tag) |
| Original data type | OriginalDataType | NodeId | (Inherited from Tag) |