OPC UA server
Publishes nodes of the information model for the OPC UA client project
- BrowseName
- OPCUAServer
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Endpoint URL | EndpointURL | ResourceUri | Communications protocol and network address of the endpoint on the server |
| Sampling interval | SamplingInterval | Duration | Time interval between successive readings of the field variables by the server |
| Maximum number of connections | MaxNumberOfConnections | UInt32 | Maximum number of OPC UA clients that can connect to the OPC UA server |
| Minimum message security mode | MinimumMessageSecurityMode | Message security mode | Minimum security level for messages exchanged between client and server. None = the messages can be unsigned and unencrypted; Signature = the messages must be signed or signed and encrypted; Signature and encryption = the messages must be signed and encrypted |
| Minimum security policy | MinimumSecurityPolicy | Security policy | Minimum security level for messages exchanged between client and server. None = the client does not require any specific security policy; Basic256Sha256 = this policy or more secure; Aes128_Sha256_RsaOaep = this policy or more secure; Aes256_Sha256_RsaPss = this policy |
| Server certificate file | ServerCertificateFile | ResourceUri | Server public certificate file, according to standard X509v3 and with .der extension. It must be found in the FTOptixApplication/ProjectFiles/PKI/Own/Certs folder. If specified, the private key must also be specified. If not specified, it is automatically generated at runtime in the FTOptixApplication/ApplicationFiles/PKI/Own/Certs folder |
| Server private key file | ServerPrivateKeyFile | ResourceUri | Server private key file, with ASCII Base64 encoding and .pem extension. It must be found in the FTOptixApplication/ProjectFiles/PKI/Own/Certs folder. If specified, the certificate must also be specified. If not specified, it is automatically generated at runtime in the FTOptixApplication/ApplicationFiles/PKI/Own/Certs folder |
| Product URI | ProductURI | String | URI that globally identifies the software |
| Product name | ProductName | String | Name of the software |
| Manufacturer name | ManufacturerName | String | Name of the software manufacturer |
| Max array length | MaxArrayLength | Int32 | Maximum accepted number of elements in an array |
| Use node path in NodeIds | UseNodePathInNodeIds | Boolean | If enabled, the server publishes NodeIds with the node path inside |
| Nodes to publish | NodesToPublish | Configuration | Configuration of the nodes to be published and the users to publish them to |