Configuration
Nodes to be published via OPC/UA
- BrowseName
- NodesToPublishConfigurationEntry
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Publish dynamic configuration | PublishDynamicConfiguration | Boolean | False: publish only objects and types, True: publish also the dynamic properties of objects and types (such as DynamicLinks, converters, etc) |
| Nodes | Nodes | Node pointer | List of nodes to be published |
| Users | Users | Node pointer | Users with access privilege to this node |